(0)| 1/18/2024 3:50 PM | |
|
Posts: 10 Rating:
|
When I connect the Modbus Slave with the PLC program my Input Data works perfectly, but the Coil Output and Hold Register appears the error 8200 and I have no idea why. Also the Hold Register number matches with the PLC program DB, but the Coil doesn't. Here are some print screens:
Attachmentpng2pdf.pdf (1138 Downloads) |
| 1/19/2024 8:35 AM | |
|
Joined: 8/12/2021 Last visit: 12/10/2025 Posts: 351 Rating:
|
Hi! It is not recommended to use clock marks at the REQ input of an MB_Client. It can cause the request to be overwritten without finishing processing. Try removing and activating it manually to see if the error is corrected. You can find Status errorhere. |
Last edited by: Jen_Moderator at: 01/19/2024 11:06:09Text formatting optimized. If this Information really helps, you could use the Rate function |
|
Follow us on