05.09.2022 10:32 | |
Beigetreten: 30.05.2022 Letzter Bes: 12.09.2025 Beiträge: 634 Bewertung:
|
Hi tute_von_ute, Welcome to the Forum! To communicate in this forum we use English. Please send your next messages in English so that we can all understand you. Automatic translation of your message: Hello I have an OP77B here where the connection was interrupted when I tried to "reset to factory settings". Now nothing else is displayed after starting but the bootloader. Is there any way to bring the OP back to life? Greetings Stefan As a solution I recommend you to check the following information: How do you backup/restore with a Windows-based panel? I'm afraid if this doesn't work you may need to repair your panel. |
If this information really helps, you could use the Rate function. |
|
07.09.2022 13:15 | |
Beigetreten: 03.08.2009 Letzter Bes: 12.09.2025 Beiträge: 16409 Bewertung:
|
Hello tute_von_ute It could be that you can perform the reset to factory settigs again: https://support.industry.siemens.com/cs/ww/en/view/19701610 to do this you need a RS232 nullmodem cable like 6ES7 901-1BF00-0XA0 usualy you should be able to do so also if there is a damaged OS on the panel Bye Murof |
If this Information really helps, you could use the Rate function |
|
Folgen Sie uns auf