12/7/2021 7:43 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello brkykrbs, The official langauge in this forum is English so please post your query in English langauge here. Translataion of your post is as below. Hello guys In my Sinumerik 840D sl 11-axis machining center, I get an alarm saying "(26106)Encoder 2 axis W1 not found" and I cannot control the machine. It does not allow movement. The cables from the driver to the encoder have been checked, there is no problem, but the problem is still not solved. Waiting for your help Thank you Reply is as below - From your description it is external encoder of W axis. Which type of encoder it is? i.e. rotary or linear? How is it interfaced? via SMC? If via SMC, is 24V DC available at SMC? How you checked the cable? Please check all above points. |
Follow us on