11/26/2021 5:51 PM | |
Joined: 2/6/2020 Last visit: 5/22/2025 Posts: 26 Rating:
|
Hello, we have problem with Deckel Maho DMC63. After power ON power supply ER and inverters get two faults that do not resets: 600300 feed lock Z axis 600350 FD-LK-Z controller inhibit Then moving axis by hand, shows value only X axis encoder. Also there's one interesting moment, then tey to exit Shopmill to CNC ISO get warning- Cannot be exited: Programm or spindle active. Even in Jog mode and feed is OFF. Y and Z is on aditional FDD. Tried to change all cables in places between then or even disconnect, nothing. Attached file with photos. Any ideas there can be a problem MPI, Controller, Program and how to check to replace right part? Best regards, A AttachmentzAxisProblem.zip (500 Downloads) |
Last edited by: Allwe at: 11/26/2021 17:57:49Last edited by: Allwe at: 11/26/2021 18:51:45 |
|
Follow us on