12/16/2021 9:29 AM | |
Joined: 7/4/2017 Last visit: 8/21/2025 Posts: 18 Rating:
|
Hello, Thanks again for your support! I have already checked the digital inputs from the operation mode rotary switch, I0.0, I0.1, I0.2, I0.3, and the ones from the axis joystick switch, I1.6, I1.7, I2.6, I2.7 and they are ok( PLC status->input byte). My problem is that the axis direction inputs are not used inside of the PLC program. Also, inside of the PLC program it's available only the MDI and Auto operation modes. So, I don't know how the operator used to make the axis reference, in reference mode, and also how he used to move the axis in jog mode. "put back in function this machine": the previous owner claims that the machine used to work in the past. For the last 3-4 years the machine was not used and since some time now I am trying to put it back in function. "Internal operation mode selection": I found a documentation of Sinumerik 810M controller, I was not able to find something like that for Sinumerik 820T. In that documentation it is explained that there are 2 ways how you can activate one of the operating modes: * selection of operating modes with internal machine control panel (please check pag.55 from the attached pdf file); * selection of operating modes with external machine control panel (please check pag.58 from the attached pdf file ) I didn't know about PLC MD2002, I will check bit number 3. and I will give you a short feedback. Thanks again! Attachment362_810M_GA2_Operating_and_Programming.pdf (395 Downloads) |
12/17/2021 8:49 PM | |
Joined: 10/17/2007 Last visit: 9/6/2025 Posts: 4437 Rating:
|
You are quit lucky--more than 2 to 3 years, 820T still keeping parameters Not lost!! and now I know you mean--Internal MCP (MCP=Machine Control Panel) 820T/M is 98% same as 810T/M if in same version. 820T/M only starting from Basic Version 2 important 820T/M can only use External MCP so you no need to know Internal MCP You post manual for OP and Prog. you mostly need Installation or commission manuals please search by Google and download. I post here is "Lists" like hand book, which is "All-in-one" but no explanations, you need search for detail ones I know 820M/T from the 1st year it being developed and a lot of cases for customer services. please go ahead to ask questions. Next time you post, one picture of you 820T system front PS: if you want to deep research you also need manual for PLC interface signals and PLC HW Attachment344_810_820_GA3_Installation_Lists.pdf (406 Downloads) |
Last edited by: nulizhang at: 12/17/2021 20:53:53I know 820 very well Last edited by: nulizhang at: 12/17/2021 21:20:17If you like my comments please |
|
Follow us on