(2)| 1/6/2022 2:50 PM | |
|
Joined: 10/17/2007 Last visit: 1/21/2026 Posts: 4580 Rating:
|
#2--using Xon/Xoff is NOT HW handshaking but software handshaking --you can search by Google to clean this topic Now your problem, you need provide information as more as possible. You need to know what is X on and X off Character in Hex format from the transfer SW in your PC I will check Siemens 810T X on X off code for you . more questions: Q#1 you or anyone in your group used to make good transfer from PC to 810T ? if yes what is the last time it was good. and what have been changed? Q#2 make sure your cable is good, open to check RS232 cable ( is it 3 wires? or 5 wires? or 7 wires?) pinout you can Google it Q#3 who make the solution --I mean use transfer software under dos in PC to transfer NC program to 810T, can you contact them to help? updated 11:00 Jan. 6 EST .-- If you are sure the cable is good and no one change setting from PC side. I guess the more possible problem is someone changing 810T setting Data. as you use non Siemens SW in PC so I can only help you from Siemens 810T side, see post 800 system setting data you no need worry about 5013 it is for output. please post your 810T screenshot for SETTING DATA if you can find X on X off code in PC SW setting , compare them with SD 5014/SD 5015
AttachmentSetting_Data_COM1_mdf.pdf (381 Downloads) |
Last edited by: nulizhang at: 01/06/2022 17:08:40updated with setting data If you like my comments please |
|
| 1/7/2022 11:01 AM | |
|
Posts: 3 Rating:
|
Q#1 you or anyone in your group used to make good transfer from PC to 810T ? if yes what is the last time it was good. and what have been changed? A#1 I made good transfer from PC to 810T many times. The problem started when we changed cable, and when we put old cable back, it don't work. Q#2 make sure your cable is good, open to check RS232 cable ( is it 3 wires? or 5 wires? or 7 wires?) pinout you can Google it A#1 Thanks to your question, we found out that one wire is off., see the picture. PC (9 pin) – 810T (25 pin), 3 wires 2—4 brown 3—3 green 5-- ?? white To which pin should we put the white wire? The new cable is totally different. 1—4 brown 2—2 red 3—3 orange 4—5+6 yellow 5—7 green 6+8--20 blue 7—8 black 8+6 pink 9 no wire Q#3 who make the solution --I mean use transfer software under dos in PC to transfer NC program to 810T, can you contact them to help? A#3 This is not possible anymore, since the program is very old. updated 11:00 Jan. 6 EST .-- If you are sure the cable is good and no one change setting from PC side. I guess the more possible problem is someone changing 810T setting Data. as you use non Siemens SW in PC so I can only help you from Siemens 810T side, see post 800 system setting data you no need worry about 5013 it is for output. please post your 810T screenshot for SETTING DATA A#4 I am posting you Setting data. This pictures are made 1 day before the problem. Also there is one manual with the transfer instruction. if you can find X on X off code in PC SW setting , compare them with SD 5014/SD 5015 A#5 I do not now hot to find the x on x off code settings.. I tried in bios but there is nothing, and I can not find it in the software. Best regards, Dino Attachment810t SD and Cable.docx (354 Downloads) |
Last edited by: domerspa1 at: 01/07/2022 12:54:14Last edited by: domerspa1 at: 01/07/2022 12:54:41 |
|
Follow us on