2/21/2022 9:31 PM | |
Joined: 1/18/2022 Last visit: 3/3/2025 Posts: 11 Rating:
|
Hello, I'm migrating an old machine that has an old incremental encoder from a defunct company to a new system that consist of an S7-1214c PLC to use the built-in HSC inputs to read the encoder pulses. But the problem came when i measured the voltage output from the signal line of the encoder with a multimeter which showed that the pulse train is 5VDC. Now i need to adapt this signal to 24VDC to use it with the HSC input on the PLC but i'm lost a bit because i've never tried something like this before therefore i'm here asking for advice I measured the pulses frequency of the signal line when the machine was running and the encoder gave a steady rate of around 100Hz, so my first reaction was using a solid-state relay since the frequency isn't that high and some solid-state relays have higher switching frequency than this; So would buying a solid-state relay like TOS 5VDC/48VDC 0,1A work? It's an optocoupler with a rated control voltage of 5VDC and a max switching frequency of 3000Hz and the rated switching voltage on the load side is 5-48VDC. Any input would be appreciated, thank you for your time! Best regards, safar |
Follow us on