4/11/2009 5:47 AM | |||
Joined: 9/27/2006 Last visit: 9/12/2025 Posts: 12407 Rating:
|
Hello Mohamad; If you are very new to S7 PLCs, the best suggestion I have is for you to sit down with some basic information and start reading. If you have worked with other brands of PLCs then your learning curve will require some work; if this is a totally new environment for you, I do not recommend that you start without some training or at least good information. Here are a few items I can recommend to start with: Working with Step 7: http://support.automation.siemens.com/WW/view/en/18652511 S7-300 Installation and operations manual: http://support.automation.siemens.com/WW/view/en/13008499 Programming with Step 7, v. 5.4: http://support.automation.siemens.com/WW/view/en/18652056
or some kind of MPI/Profibus communication processor for your programming PC, CP 5512 (PCMCIA card), CP 5611 (PCI Softnet), CP 5613.... Hope this helps, Daniel Chartier |
||
Follow us on