4/27/2009 11:36 AM | |
Posts: 325 Rating:
|
Hi All, Below is the link for the FAQ reg. "Additional Authorization Levels in Standard Faceplates". http://support.automation.siemens.com/WW/view/en/21571145 Tried this but didn't work. More over I am bit stuck at one point ( Page 15/16 in the FAQ). Along with the FAQ there are only 3 scripts which are to copied and re-compiled "pcs7_updatepermission_v6_mj, pcs7_opengroupdisplay_v6_mj and pcs7_openloopdisplay_v6_mj". The FAQ at page 15/16 says PCS7_UpdateLoopTagname_v6_MJ(.....). This script couldn't be found. Can any one help me plz..... Regards Nil96 |
Follow us on