11/14/2022 6:16 AM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, As you found out, if you want to have redundant I/O the only module you can use is the ET200 SP HA. In the following overview, you can find all Profinet modules with their functionality. As you can see, the ET200 SP HA has the following advantages:
PA ready basically means that I/O modules have unlimited use without restrictions especially needed in Process Automation. There is a special icon to indicate this and is compromised of the following:
In the following manual, you have a complete overview of Profinet. One of the first links is the Guidelines and Blueprints where you can find information about Profinet as well as example setups. Profinet in Process Automation with PCS 7
|
Last edited by: Oreca at: 11/14/2022 06:52:20Last edited by: Jen_Moderator at: 11/14/2022 07:47:26Links optimized. If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
2 thankful Users |
Follow us on