11/19/2022 11:07 AM | |
Joined: 1/11/2019 Last visit: 8/14/2025 Posts: 899 Rating:
|
Hello Ashadako,
Few IOs of block like Bad, Mode.. of channel drivers works properly with actual CPU not with Simulator (PLCSIM) The actual CPU gets the PV signals and Diagnose signal from connected IOs If your are testing with actual CPU and still getting Bad signal =1 one even after setting Simon=1 the please update your PCS7 V9.0.3 to PCS7 V9.0.3.5 (Update collection 5) Below is the link for PCS7 V9.0.3 Upd5 Note: My systems are updated with PCS7 V9.0.3 upd5 and it is working fine. |
This contribution was helpful to
1 thankful Users |
Follow us on