11/28/2022 6:09 PM | |
Joined: 6/1/2020 Last visit: 8/21/2024 Posts: 41 Rating:
|
I have a TP1500 panel and I would like to save the logs in a shared folder instead of the SD card. I have seen that I could use HMI Option+ to do that: https://support.industry.siemens.com/cs/ww/en/view/92346478 In the documentation, it is said that when HMI Option+ copy the file from the SD to the shared folder, the file in the SD card is deleted. Does it mean that HMI Option+ ensure before deleting than the file is copied in the shared folder? What happen if the shared folder is not available? One reason it is because Windows 10 decides to reboot. I have seen in the documentation that Windows 10 is the operative system used in the examples, and Windows can't ensure 24/7 availability, because sometimes it decides to reboot, normally because of updates. If the shared folder is not available, does HMI Option+ try to copy later when the shared folder is available again and then is when it delete the file from the SD card? Thanks. |
Last edited by: Jen_Moderator at: 11/29/2022 08:23:26Link optimized. |
|
Follow us on