1/27/2023 4:41 PM | |
Joined: 7/11/2012 Last visit: 7/1/2025 Posts: 3 Rating:
|
Hello, I am glad to find this conversation about "Module error entering state". I have the same problem in our PCS7 system. Every time, this alarm would pop up while system detected a wire break or fault. IN your previous post, "WinCC alarms use the same format to signal either the arrival of a fault in the PLC, or the removal of the fault. You can select one, both or none of these signals to trigger an alarm in your alarm display." But I have no idea how can I select to not show "Module error entering state"alarm? I need immediate help because operator was bothered by this alarm every couple minutes when maintenance has not fixed wiring. system: PCS7 V8.2 SP1 WinCC: V7.4, SP1, UPD6 Thank you in advance Winston Liu ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/08/2023 11:15:32New subject after splitting |
|
2/8/2023 11:16 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject How to disable alarm 'Module error entering state'? is published within the conference Process Control Systems SIMATIC PCS 7. Jen_Moderator |
Follow us on