3/2/2023 2:30 PM | |
Joined: 5/9/2011 Last visit: 10/10/2024 Posts: 1 Rating:
|
Hello, I have a question about the Maintenance Station package which is used to display the status of PC's (ES/OS), network switches and PLC's on PCS7 via SMTP. The PCS7 system is version 7.1 SP2 (1x ES, a redundant OS and 8 clients). My method to visualize these objects (see also the appendix for more details):
The WinCC tags (SMTP"_...) are properly created in the WinCC Explorer. After the above mentioned actions everything is displayed correctly on the 3 PCS7 diagnostic screens ("PC stations", "Network Objects" and AS objects"), but not for 7 clients, only 1 is good, but I see no differences with the other 7 in terms of configuration. Also a red wrench is shown for the 7 clients and an alarm message: "SNMP device is not answering". The SMTP Windows component is installed on the clients. Does anyone have an idea what could go wrong here? Thanks in advance, Ben AttachmentMaintenance Station.docx (304 Downloads) |
Follow us on