3/3/2023 7:05 AM | |
Joined: 5/3/2017 Last visit: 2/6/2025 Posts: 673 Rating:
|
Hi La masa, in PCS 7 you have the same opportunities to create a block as STEP 7, also with LAD/FBD/STL and SCL. The step-chain are implemented with SFC which similar to S7-GRAPH. But before you begin to write all blocks itself, PCS 7 offer the installation setup CEMAT with is specially designed for the mining industry. Siemens offers a demo project with CEMAT, see the application example SIMATIC PCS 7 in the mining industry (demo project). With regards |
Last edited by: Heisenberg2 at: 03/03/2023 07:06:51 |
|
This contribution was helpful to
1 thankful Users |
Follow us on