6/20/2021 10:10 PM | |
Joined: 3/14/2008 Last visit: 9/4/2025 Posts: 2216 Rating:
|
Hi, The driver block has connection to the hardware and some signals like Mode are sent from hardware to the block in case of using "Generate Module Drivers" function. They are created automatically. For example Mode will show if the signal is 4-20mA or 0-10mv etc. If you want to simulate, either delete the module driver connections or a better way use simulation (SimOn). The system automatically checks option: Generate Module Drivers during each compile so you have to deactivate it each compile if you don't want to use this function |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
Follow us on