10/13/2017 3:21 PM | |
Joined: 3/14/2008 Last visit: 9/8/2025 Posts: 2216 Rating:
|
Hi Amen Allah, There are a few posts on the subject. There is a FAQ that states that you may reinstall SQL server after an instance of WinCC is started, but that doesn't apply to PCS7. PCS7 is more difficult in that matter. For PCS7 you must use the restore DVD which is supplied by the IPC. But, if you installed PCS7 on a "regular pc/notebook" by yourself, you must reinstall from scratch-> Install Windows, set the correct computername, then install PCS7. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
10/13/2017 4:01 PM | |
Joined: 10/26/2011 Last visit: 9/4/2025 Posts: 765 Rating:
|
If you didn't start the SQL Server and SIMATIC Manager or other components, which use the SQL server inside, then you can rename the computer. Otherwise, you have to reinstall everything. |
SIMATIC PCS 7 - Overview |
|
10/13/2017 4:54 PM | |
Joined: 3/14/2008 Last visit: 9/8/2025 Posts: 2216 Rating:
|
Sorry Thunderstorm, From the PCS7 Compendium part A PCS7 V8.2: Changing computer names So, I would not recommend changing the computername in a production plant, but changing the name for one of your test ES systems should be possible with regard of above conditions. |
If I could help you, you can use the RATE button. Thank you. |
|
4/5/2023 11:24 AM | |
Joined: 9/9/2015 Last visit: 4/9/2025 Posts: 732 Rating:
|
In case you are doing it for test environment, may look at this method. Hope it helps |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on