3/28/2023 12:38 AM | |
Joined: 9/9/2015 Last visit: 4/9/2025 Posts: 732 Rating:
|
Hi, Yes, "Group relevant" feature will definitely work. However, the alarm did not show on the group display. I was exploring to change the graphics pdl name to trick the AS-OS engineering system, by changing the PDL name to arrange in the front instead of the back. However, this is still under testing. Another method is changing the tagname attribute, adding "Server Prefix" in front. For example, if the tag name is 123PT1234/MonAnL , then i will add SERVERPREFIX::123PT1234/MonAnL at the duplicated block icon to trick the AS-OS engineering. Last resort is, changing directly at component list editor in WinCC Explorer. Hope this helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on