11/20/2023 11:13 AM | |
Joined: 12/20/2017 Last visit: 9/2/2025 Posts: 1 Rating:
|
As explained here https://support.industry.siemens.com/cs/de/en/view/109482823 I'm tring to show a page loaded from usb stick. Using the path ""/media/usb/USB_X60.1/index.html" give as output "The requested page (file:///media/usb/USB_X60.1/index.html) could not be found. Error code: 203" What I am missing? Is it the address incorrect? How can I fix? |
Last edited by: The Helping Hand at: 11/21/2023 08:22:27Link optimized |
|
11/20/2023 12:21 PM | |
Joined: 7/19/2022 Last visit: 9/11/2025 Posts: 436 Rating:
|
Hello FioDeDevi, It is likely that the USB is not recognizing it. Try setting up an alarm viewer to view system alarms to see if any error messages appear. Also try using a low capacity USB |
If this Information really helps, you could use the Rate function |
|
11/20/2023 1:02 PM | |
Joined: 4/26/2012 Last visit: 9/9/2025 Posts: 1645 Rating:
|
Hello, Hello, welcome to the forum in the documentation in your link it says .htm you are using .html tried to change Which HMI model are you using? Errro code 203 to read LINK Try it like this, I only tested it in the simulator.
c://teste.htm I realized that accents in words, has trouble identifying. Note For Basic Panels 2nd Generation: If you want to load a website from a USB flash drive to your HMI device, the address in the "URL" field must begin with the prefix "\media\usb\". Example: You want to load the html5.htm web page from the USB device USB_XY. Enter "\media\usb\USB_XY\html5.htm" in the Inspector window. good luck.
|
Last edited by: rdoliveira at: 11/20/2023 13:08:27Last edited by: rdoliveira at: 11/20/2023 13:11:10Last edited by: rdoliveira at: 11/20/2023 13:13:52edit Last edited by: rdoliveira at: 11/20/2023 13:40:28Last edited by: rdoliveira at: 11/20/2023 13:42:44Last edited by: rdoliveira at: 11/20/2023 13:46:57"Always make a backup before performing any tests |
|
Follow us on