12/16/2009 9:55 AM | |
Posts: 159 Rating:
|
Hello! Yesterday I wanted to try out the reorganize function in Simatic manager that I read som much good about, "its like defrag your disc etc.". So I closed my project down (wincc, simatic manager etc)and restartet simatic manager, and startet the reorganize function by file-->Reorganize. Everything seemed to work well, except when I tried to open my multi project again! When I try to load the multiproject I get this error saying "Can not read hierarchy folder"! When I acknolwledge this message with the ok button, then it dissapear. But all I can see in my subprojects (plant view) is the shared declaration folder. Im missing the hierarchy folders! Does this mean that the "Reorganize function" has wiped all my hierarchy folders in the multiproject?? I have rebooted and started up again with the same error. My installation is PCS 7 v7.0 on an xp machine. I have two project in a multiproject. One pcstation as an es_os (singlestation) Please help! Attachmenterror.zip (262 Downloads) |
Last edited by: Testermax at: 12/16/2009 4:38 PMLast edited by: Testermax at: 12/16/2009 12:43 PM |
|
12/17/2009 9:45 PM | |
Posts: 3149 Rating:
|
Hi did you already try in Simatic Manager "Save as > with reorganization"? I think this is the functionality you intended to use... nemo |
8/22/2012 10:25 AM | |
Posts: 7 Rating:
|
Hi....i have the same issue now....do you have solution for it?? if please do share with me. Thanks.
|
Follow us on