10/10/2024 8:08 PM | |
Joined: 7/31/2024 Last visit: 2/15/2025 Posts: 5 Rating:
|
I want to start the MCP 416 that I have. (It is built into the original DMG operator panel). I wonder what the problem is. I plan to replace it with CCU3, I even bought it already but there was a problem. The purchased CCU3 SW 6.3 after installation starts, goes to 1 -> 5. -> 5 -> 6 on the display, the diodes +5V green, SF red, PR green light up. PS red and, and PF flashes red. I wanted to upload a copy of NC and PLC but unfortunately I can't clear NC or PLC through switches SW3 and SW4. There is no reaction to changing the positions of SW3 and SW4. There is also no communication from the PCU50 and MMC103 level. Is it possible that I need a PCMCIA card with 810d firmware? |
Last edited by: @AutoGen_860549 at: 10/10/2024 20:52:37 |
|
10/11/2024 6:52 PM | |
Joined: 10/17/2007 Last visit: 9/18/2025 Posts: 4455 Rating:
|
#1 You make simple things completed --are sure you can upgrade you machine system from CCU1 to CCU3 ? #2 from your 1st question page, you never post any picture that would be very hard for other people to help you--we can only using imagination to think very hard what was happening 810D CCU1 and CCU3 are all discontinued by Siemens for years, no more support , you make OP012 +PCU50 working is good . OP032S , is better replaced by 19" MCP the number I sent to you, MCP 416 is designed for 840D/810D solution Line,
|
If you like my comments please |
|
Follow us on