11/20/2024 3:55 AM | |
Joined: 11/5/2022 Last visit: 4/20/2025 Posts: 4 Rating:
|
Hi everyone. I have a s7 1200 plc cpu1214C dc/dc/dc At last week , there is no problem. And I can connect to PLC and program it . But today, when I connect power 24VDC to it , the Error Led start to blinking (RUN led is green and ok ). In TIA V17 , I can only see IP address of plc , and I can not assign New IP address. When I try to download program to It , the following error appear: "connection failed. Selected online target is not reached....." Can you belp me to solve this problem ? (I have Windows 10 , 64bit) ------------------------------------------------------------------------------------------ |
Last edited by: EhsanNiknami13701123 at: 11/20/2024 04:03:04Last edited by: Moderator_Lan at: 11/20/2024 10:21:10New subject after splitting |
|
Follow us on