12/11/2024 10:48 AM | |
Joined: 8/1/2013 Last visit: 5/9/2025 Posts: 127 Rating:
|
Hi Steve. We face similiar problem. We have a Normal computer with Operate system (Not base). A ONE Sinumerik 1750 + HT10. The main problem is with MDA, whenever you change to MDA, ramdombly the MDA is on the HT10 and then is not possible to modify on the computer. When this happens, we open by VNC and change the screen to Startup, then on the computer we select again MDA and "eboila", the MDA bufffer move to the computer. Is not a big task, but some customers are really anoyed about that. I have a partial solution, if you select F10-F6 or startup screen, then if you press Jog, AUTO,etc. The HT10 keeps on Startup screen. and after that the MDA alwais are on the computer. What I dont know Is how can I program or modified, for example whenever i press jog or auto or MDA, change the HT10 to startup screen istead move always to Machine screen or F10-F1.... Any idea? Regards¡ ________________ split from: MDA Text is write protected |
Last edited by: Moderator_Lan at: 12/11/2024 11:02:31New question split into seperate topic |
|
12/11/2024 11:53 AM | |
Joined: 4/28/2015 Last visit: 9/8/2025 Posts: 27 Rating:
|
You have to switch off the internal HMI, |
12/11/2024 11:55 AM | |
Joined: 8/1/2013 Last visit: 5/9/2025 Posts: 127 Rating:
|
Hi, But if you disable the HMi screen by WinSCP por example the HT10 will not work |
Follow us on