6/30/2009 12:35 PM | |
Joined: 4/5/2006 Last visit: 7/30/2025 Posts: 917 Rating:
|
Hi mangesh, here some links from web support pages, FAQ:How can you clear the following error message during OS compilation: "The number of parameters for the structured DM variables xxx of type yyy does not match the number of operator-controlled connections...". FAQ:What is the meaning of the error message "A structure conflict occurred when creating the structured DM variable XXXX of type YYYY..." when compiling the OS? FAQ:How do you clear the error message "The number of external DM variables in WinCC exceeds the permitted in total number" during OS compilation? Should help you Regards |
7/1/2009 8:52 AM | |
Posts: 16 Rating:
|
thanks for your replay as i am attach the log file which genrate during os compilation and as per the log i am make requierd changes in my program but still the same error is genrated during compilation pl mark your comment on the same. AttachmentTRANSFER.zip (200 Downloads) |
7/1/2009 12:36 PM | |
Posts: 272 Rating:
|
Hi, Please check the plant hierarchy and the name of the corresponding blocks. It seems from the log that the name of the blocks are same. |
7/2/2009 7:50 AM | |
Joined: 4/5/2006 Last visit: 7/30/2025 Posts: 917 Rating:
|
Hi mangesh, as well as Phantom75said, there are duplicate TAG_NAME in your plant: In plant hierarchy it possible setup how you want compile tag_name in OS (chart/block or hierarchy/chart/block and so on).It possibile you have same "chart" & "CFC block" name in different hierarchy maybe but yo compile chart/block ONLY to OS. Have a look to project hierarchy name object and "Plcnt Hierarchy" setting, like other guys said, ....error is there Regards |
Follow us on