10/4/2024 10:49 AM | |
Joined: 7/19/2022 Last visit: 9/11/2025 Posts: 436 Rating:
|
Hello SiggiDeSmedt, I'm afraid that since the CPU has a firmware loaded that does not appear in TIA Portal V15.1, you will not be able to upload the program. In order for an upload to be 100% successful, the TIA Portal version with which it was programmed and a CPU compatible with said TIA Version are required. In this case, since V2.8 is not available in TIA Portal V15.1, it will not be possible to upload the program. |
If this Information really helps, you could use the Rate function |
|
10/4/2024 11:03 AM | |
Joined: 3/30/2020 Last visit: 9/11/2025 Posts: 5444 Rating:
|
What you say is not true. It is possible to load a PLC as if it is a lower version firmware. The online diagnostic however do report the firmware loaded into the PLC. It is not reported that it is running a in compatibility mode. It does not state which firmware version is referred to in the software. As seen in the question, the software tells you about incompatibility if that is the issue. - I do not know what the issue is. I have seen such behaviour if there is a cable issue. Other than that it is a good idea to use the "Support Request" link while waiting for more volunteers to react. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on