1/16/2025 10:38 AM | |
Joined: 3/26/2016 Last visit: 3/21/2025 Posts: 36 Rating:
|
Is there a way to view and swap to different windows open in TIA similar to step 7? |
1/16/2025 11:52 AM | |
Joined: 5/6/2022 Last visit: 9/9/2025 Posts: 589 Rating:
|
Hi Liem.Tran1, I don't know if you are referring to the option that TIA Portal offers in the bottom bar that shows 'For such a View' and that I attach as a picture. In this part you get the windows to go to the parts you already had open and with which you were working faster. Do you mean this? |
If this Information really helps, you could use the Rate function |
|
1/16/2025 12:20 PM | |
Joined: 3/26/2016 Last visit: 3/21/2025 Posts: 36 Rating:
|
Yes - thats exactly it. How do you get yours to show in parentheses what the block number is? As you see from my screenshot it's difficult to see what is what and i end up having to click on each one. |
1/16/2025 1:14 PM | |
Joined: 5/6/2022 Last visit: 9/9/2025 Posts: 589 Rating:
|
Hi Liem.Tran1, I think the option to display the block function, for example (FB2) is there by default. In your case, since you have a longer name for the FB, it does not appear. As a solution, I think you should put the FB number at the beginning of the FB name, for example "(FB2)....." In this way, the FB number will always appear first and you will be able to locate it, since the more tabs you have, the smaller they will become, and I think this cannot be modified. |
Last edited by: ElonksuM_SN_BN at: 01/17/2025 08:51:49If this Information really helps, you could use the Rate function |
|
Follow us on