1/16/2025 5:24 PM | |
Joined: 12/10/2024 Last visit: 8/8/2025 Posts: 2 Rating:
|
I'm getting the following message when running the installation file of TIA Portal v19 Some product components cannot be installed. 'SIMATIC WinCC Professional 19' cannot be operated in parallel with the currently installed version of WinCC Unified PC Engineering' or WinCC Unified If you uninstall WinCC Unified PC Engineering' via Control Panel, select 'Siemens Totally Integrated Automation Portal' and follow the wizard. Found this note: https://support.industry.siemens.com/cs/be/en/view/109822246 It says "This message is a note. Please make sure that WinCC Unified PC Engineering or WinCC Unified PC are completely uninstalled. Does this mean that WinCC Unified and WinCC Professional can only be installed in parallel on version 19, and if I have WinCC Professional/Unified from a different version, installation isn't possible? Thanks in advance |
Last edited by: Moderator_Lan at: 01/17/2025 07:43:48link optimized |
|
1/17/2025 6:13 AM | |
Joined: 5/12/2006 Last visit: 9/15/2025 Posts: 22687 Rating:
|
correct |
1/17/2025 6:48 AM | |
Joined: 7/9/2015 Last visit: 8/29/2025 Posts: 4443 Rating:
|
Hi, for further informations please check this FAQ: Requirements for installing TIA Portal V19 (WinCC Unified V19 ES and RT)Regards, Towome |
|
|
Follow us on