1/17/2025 9:27 AM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello Joseph, it could be a version conflict. The appropriate solutions are described in the FAQ: What options are available in STEP 7 (TIA Portal) for uploading when the project version in the CPU no longer matches the version on your PG/PC? Otherwise, I recommend creating a new project and uploading to the new project. There is also the FAQ: In STEP 7 (TIA Portal), how do you load the "Program Blocks" with the PLC tags and PLC data types from the CPU into the programming device? With best regards |
This contribution was helpful to
1 thankful Users |
Follow us on