7/9/2009 9:27 PM | |
Joined: 4/5/2006 Last visit: 7/30/2025 Posts: 917 Rating:
|
Hi NimaMoadelli, dilipan_csaid right, only in the PCS7 v7. there is a library with LOCAL/REMOTE functionality in Siemens standard vlock, and you have to use Advanced Prcess Library for that. In previuous versione doesn't exist that functionality and you have to build an external logic to simulate the motor command: put motor in auto and use motor running signal to simulate command, then putmotor running signal in feedback motor input but delayed one scan cicle. This works whenlocal panel connected directly in MCC, if connected in plc and plc control motor logic will be different ut same concept (put motor block in auto mode) Hope is what you wasking Regarding |
7/10/2009 9:26 AM | |
Posts: 272 Rating:
|
well local remote funcationality might be added in the OS also... |
7/10/2009 10:31 AM | |
Posts: 32 Rating:
|
Would you please explain? in details Best Regards |
Follow us on