7/12/2009 6:34 AM | |
Joined: 9/27/2006 Last visit: 9/16/2025 Posts: 12409 Rating:
|
Hello Walid; This interesting document was proposed on the forum by Bilal Moola in the following exchange; you might find it useful for the OP 73 as well: /tf/WW/en/Posts/21253 You should also look at the WinCC Flexible manual for the OP 7x family: http://support.automation.siemens.com/WW/view/en/21084916 So basically, to interface with the CPU you should look at MPI or Profibus. The easiest andmost flexibleconnections will require Profibus cable of sufficient lengthand Profibus connectors. The "RS232 / PPI Multi Master Cable" (6ES7901-3CB30-0XA0) serial cable is required to transfer project data to the OP73micro {i.e. from the WinCC Flexible PC].. Only serial transfer is possible at micro operating panels. AttachmentPanels_Possibilities_of_connections.pdf (332 Downloads) |
Last edited by: dchartier at: 7/12/2009 10:48 AM |
|
Follow us on