6/2/2022 4:07 PM | |
Joined: 5/12/2006 Last visit: 9/18/2025 Posts: 22710 Rating:
|
please expand the warning message an mak a new screen with the exact message informations |
6/3/2022 7:34 AM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi newnew0816, as already mentioned, please extend the message and create a new screenshot, as we can not see the hardware and firmware versions used. But in general, if a CPU-1500 is used, following FAQ may be helpful. How do you load the project data if the version of the firmware installed in the S7-1500 CPU cannot be selected in the hardware catalog of your version of STEP 7 (TIA Portal)?regards sancruz |
Feedback appreciated, please rate |
|
6/4/2022 5:50 PM | |
Joined: 6/2/2022 Last visit: 7/27/2022 Posts: 8 Rating:
|
This is the extended error message. I can load the programme to PLC and i am using s7-1200. |
8/6/2025 7:54 AM | |
Joined: 8/6/2025 Last visit: 8/6/2025 Posts: 1 Rating:
|
Hello! But what should I do if i want to fix it? Update HSP? |
Follow us on