9/4/2025 9:05 AM | |
Joined: 8/3/2009 Last visit: 9/18/2025 Posts: 16447 Rating:
|
Hello U_cc314cf8-879a-4... For WinCC Professional Redundancy you do not need a special configuration for the CPs. You would also be able to use common network cards. Check out the generel information in this example: https://support.industry.siemens.com/cs/de/en/view/109772627 Which kind of redundancy do you want to set up? Only a WinCC redundancy or also integration in a MRP ring or do you also have a R/H PLC? Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on