10/27/2009 9:18 AM | |
Joined: 1/4/2007 Last visit: 8/26/2025 Posts: 1190 Rating:
|
Hello grimreaper, To communicate with the Siwarex MS module, you need the configuration package CD with the order number: 7MH4930-0AK01. On that configuration package CD, you can find the Siwatool software to communicate between the Siwarex MS module and a PC. You can download the Siwatool-Demoversion by logging on to: http://support.automation.siemens.com/WW/view/en/22601567 Also you can find on that configuration package CD two libraries, which you have to link to the MicroWIN software. There exist a Step7 example program ("Getting_Started_CPU222_TD100C.zip")into the internet for the Siwarex MS module: http://support.automation.siemens.com/WW/view/en/22605342 Also I recommend to you to read the chapter 8 (=Communication with Step7) of the manual of the Siwarex MS module. You can download the manual of the Siwarex MS module by logging on to: http://support.automation.siemens.com/WW/view/en/22600601 Bestregards Siwarexi |
Last edited by: Siwarexi at: 10/27/2009 9:20 AM |
|
Follow us on