4/12/2011 9:46 AM | |
Posts: 1 Rating:
|
bon jour siwarexi j'ait un siwarex ms et je vouliez comment configure le dans cpu Splitted from SIWAREX MS callibration. |
Last edited by: O_Moderator at: 4/12/2011 11:30 AMnew subject after splitting |
|
4/12/2011 4:06 PM | |
Joined: 1/4/2007 Last visit: 8/26/2025 Posts: 1190 Rating:
|
Bon jour djouada, parce que mon francais est tres mal, je recrire en anglais … Well, it is quite easier to configure the Siwarex MS module via the Siwatool software. You can find a Demoversion of the Siwatool software on the internet: http://support.automation.siemens.com/WW/view/en/22601567 Also there exist a Quick Guide how to configure the Siwarex MS module via the Siwatool software: http://support.automation.siemens.com/WW/view/en/40965488 But if you want, you can also configure the Siwarex MS module via Step7. Into the manual of the Siwarex MS module: http://support.automation.siemens.com/WW/view/en/22600601 you can find into chapter 8.9.2 an example how to read/write data from/to the Siwarex MS module, e.g. the adjustment weight. Into the chapter 8.9.1 you can find an example how to send a command (e.g. “Tare”) to the Siwarex MS module. There exist a Getting Started Step7 project with one TP177micro-Panel: http://support.automation.siemens.com/WW/view/en/22605342 Best regards Siwarexi |
Follow us on