4/25/2011 12:44 AM | |
Joined: 3/28/2010 Last visit: 9/17/2025 Posts: 1172 Rating:
|
FC070 documentation is available here: prim=0&extranet=standard&viewreg=WW&objid=23781606&treeLang=en
prim=0&extranet=standard&viewreg=WW&objid=23781606&treeLang=en Page 66 of the FC070 manual shows the FC070 wiring for either RS-232 or RS-485.
example is shown on page 68, complete with jumpering. RS-232 wiring is shown on page 69.
port > COM 4) which is available in Windows' Device Manager.
MUST match on both the PC and the FC070. I don't have a copy of PDM here, so I can't be specific where the PDM's COM port settings are but it is a tabbed location under properties, if I recall correctly.
|
Follow us on