6/9/2011 11:00 AM | |
Joined: 7/2/2008 Last visit: 8/7/2025 Posts: 928 Rating:
|
Hello Tomy Master
To the best of my knowledge you won't find IP68 in Siemens. You can find IP65 (water jets)and sometimes IP67 (immersion up to 1m) but didn't see IP68(immersion beyond 1 m) in the catalog before. Is your application that special? Anyhow, you can download the FI (field instruments) catalog from this link. Best regards. H-H |
This contribution was helpful to
1 thankful Users |
6/10/2011 1:49 AM | |
Joined: 5/4/2009 Last visit: 11/23/2024 Posts: 914 Rating:
|
OK Would you please show me the closest solution to the specification. Regards Tomy. |
Aim Higher |
|
Follow us on