8/12/2012 9:07 AM | |
Posts: 2964 Rating:
|
Hello... Yes your right "S" is stepper.... The pulse setpoints of the CNC are interpreted in the drive position controller and transferred as speed setpoints . TTL encoder feedback of the connected 1FL5 servomotors leads to significantly incereased dynamic behaviour than is possible with the stepper motor applications... Check the PDF 802S with V60 Drive,,,, Regards, Prakash Attachment802s_V60.pdf (154 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on