8/10/2012 6:51 PM | |
Posts: 2964 Rating:
|
Hello... |
8/11/2012 10:18 AM | |
Posts: 7 Rating:
|
Thanks for your reply Prakash terminal 112 & 9 was by default already jumperd and 1u1,2u1,1v1,2v1,1w1,2w1. As far i know i got all terminals connected of the infeed. Exept terminal X111(74,73.2,73.1,72) X121(5.3,5.2,5.1). Not sure if it's also needed For the moment i'm testing it through 3~ 230V inverter or else for 380 i have to bring the system to the workshop. Yes i've tested before on 380V. MD Drive i've added the power module and the motor types, and in MD General,MD Channel and MD Axis has being automatic adjusted afther i add the motor and modules. The encoder selection i have chosen the with absolute measuring systems (EnDat interface) I have added your code into the OB1 and "PLC pulses enable" shows now a "1" it seems like it works! But is it correct?and does this code only for the X axis? I can send you my project from step7 most components already added but. I'm not a that skilled PLC programmer t. I mostly know the LAD language but than S7 1200 PLC's Thanks Regards, Paul |
Last edited by: ThePDI at: 8/11/2012 10:19 AM |
|
Follow us on