4/30/2015 8:30 PM | |
Joined: 10/12/2014 Last visit: 3/17/2025 Posts: 66 Rating:
|
My hardware configuration is one 115 cpu u get I / O from 2 remote stations (ET 100 Distributed I / Os). This 2 remote stations (ET 100u) connect with separate 2 serial links via 308-3UA12 Expansion Unit Interface Module. My fault IS I can not operate 2 et100 u stations Simultaneously .At one time this can operate only one.This Means i stop one manually by ON / OFF switch, then other station can ON.Then i ON the OTHER off station there flashing I / O disable bulb in red. Here I attach i stack and B stack and hardware configuration . And other is In remote stations there display inputs(flash in green) , but after check i online cpu via step 5 software there not display the ' 1 ' statues . My understanding figure is erase eprom program on 308-3UA12 Expansion Unit Interface Module .Can it happen ..??? Can u send me sir COM ET 100 communication software ??? I couldn t find this software from internet.
AttachmentATTCHMENET22042015.zip (457 Downloads) |
5/4/2015 9:59 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4759 Rating:
|
|
Follow us on