4/27/2016 12:28 PM | |
Joined: 11/21/2007 Last visit: 7/25/2025 Posts: 2326 Rating:
|
Hello Pl see the replies to similar question in the following threads : Need help on S5 Instruction Need Support for Convertion S5 - S7 Additionally pl note : OB 255 -Transmit data block from the user program memory into the data block RAM The FB is copying selected DBs from EPROM to DB RAM. I don't think you will need this code in S7. You can discard this Block and its calls. Hope this helps Cheers Navnag |
Last edited by: Navnag at: 4/27/2016 12:32:38 PMThere is no such thing as the last bug in a program |
|
Follow us on