3/31/2014 6:24 PM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Hi, As from STEP7 V13 it is possible to upload an S7-1500 to PG/PC, including software, comments, symbolic information and hardware for S7-1500 (central modules and distributed periphery). To upload the project, it is necessary to have a connection with the PLC (test it with “online access”) and to open a project first (I suggest to create a new project as organization reason). After that, select the menu option “Online”->”Upload device as new station (hardware and software)…” The follow cast shows this procedure. AttachmentC:\Users\z0008iwv\Documents\Bluetooth Exchange Folder\upload.zip (1425 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
4 thankful Users |
Follow us on