10/26/2017 8:22 AM | |
Posts: 1 Rating:
|
Hello , I have all the time LOE( The PROBE Milltronics P130945) , even when sensor is out of tank . Can you explain procedure to make rST ( factory reset ). When I 're in position of rST and press 4 or 20 it show on display range of possible numbers from 1 to 10 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/26/2017 8:29:56 AMNew subject after splitting |
|
11/13/2017 3:17 PM | |
Joined: 12/13/2012 Last visit: 10/5/2023 Posts: 124 Rating:
|
Hello, there is no "factory reset" parameter for "THE Probe". I suggest to do a new start up to overwrite the old settings. If you get a "LOE", also if you put the Probe directy in a direction to a wall out of the silo, the unit seems to be damaged. What kind of application is it ? Is there ammonium present in the atmosphere ? ------------------------------------------------------------------------------------------------------------------------- Hello , I have all the time LOE( The PROBE Milltronics P130945) , even when sensor is out of tank . Can you explain procedure to make rST ( factory reset ). When I 're in position of rST and press 4 or 20 it show on display range of possible numbers from 1 to 10 ------------------------------------------------------------------------------------------ |
5/30/2018 3:34 PM | |
Posts: 2 Rating:
|
|
Follow us on