7/31/2018 2:30 PM | |
Posts: 11 Rating:
|
Dear Caod , Thanks a lot for your support.Yes, I have checked in Wincc Flexible PC S5115u CPU941/942 TTY/422 relate to S5 AS511 is present. Regards Talha Sohail |
8/2/2018 12:24 PM | |
Joined: 12/1/2009 Last visit: 7/14/2025 Posts: 672 Rating:
|
Hi, There are many manufactures offering HMI's to communicate with S5 through AS511. So here is another one: Panels: http://beijerinc.com/product/industrial/index.php Drivers list: http://beijerinc.com/product/ix/drivers.php Good Luck Best Regards. Communication performance of AS511: Don't expect a fast data exchange between the S5 and the HMI when using AS511. In order to increase the performance arrange all data in one area without big gaps and don't spread it over the whole address memory of the CPU if possible. |
Last edited by: TIBI68 at: 8/2/2018 12:32:39 PMGive us your feedback and show us your respect! |
|
8/3/2018 9:30 AM | |
Posts: 11 Rating:
|
Hi, Thank you for your support |
Follow us on