10/10/2024 4:21 AM | |
Joined: 10/9/2024 Last visit: 6/13/2025 Posts: 12 Rating:
|
These are files that should be original to the machine, I don't understand Siemens' naming logic, but from what I observed, the files do not have headers that start with "%", the file named PCL I believe is what you call PCP, I didn't identify what L888 would be or the other so-called subprogramsX Attachmentparmetrosdafamupmcx700.zip (325 Downloads) |
10/10/2024 4:30 AM | |
Joined: 10/9/2024 Last visit: 6/13/2025 Posts: 12 Rating:
|
These are files that are from a machine from the same manufacturer said by the seller to be identical to the X700 only with larger axes, model x1000. I think there is some accessory that would be different, because looking at the original PCA file of the X700, which is the machine I am analyzing, the file in Portuguese shows an alarm from the chip conveyor that the machine has attached, already in the PCA file of the x1000 which is loaded into memory in English does not have the chip alarm code. I didn't try to load the x700 files again because I don't know if they are in good condition and it could make the machine's situation even worse, since the purchase agreement has not yet been finalized.
Attachmentparmetrosdafamupmcx1000comcomandosiemens810ga3.zip (327 Downloads) |
10/16/2024 2:44 AM | |
Joined: 10/9/2024 Last visit: 6/13/2025 Posts: 12 Rating:
|
let's go. I think now with the information we can continue. thank you. very much |
10/22/2024 1:49 AM | |
Joined: 10/9/2024 Last visit: 6/13/2025 Posts: 12 Rating:
|
Alarm=8 Message from nc = ord 1, wrong axis / spindle assign. |
11/28/2024 12:47 PM | |
Joined: 10/17/2007 Last visit: 9/9/2025 Posts: 4443 Rating:
|
You are talking about to branches--SMODRIVE and SINUMERIK #1--you have SIMODRIVE 611A , and power supply module any type you can use without problem --if they are good functional. 611A is easy to test --I will send you a manual . basically you can use battery box (suggest 1.5 VDC) to terminals 56/14 and enable 633,65, the axis should running #2--CNC 810M, if you load good back up, ( I think I told you ) you have problem for "FEED disable"--RED LED on the 810M front panel on, --it needs PLC program troubleshooting why axis "enable " signal not coming --such as machine hit limit switch , or you machine hydraulic system not working? Attachment57453743611A_IA.pdf (370 Downloads) |
Last edited by: nulizhang at: 11/28/2024 13:11:33If you like my comments please |
|
Follow us on