3/18/2022 12:33 PM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Have you checked points mentioned in my reply in this topic.? |
3/18/2022 12:52 PM | |
Joined: 3/16/2022 Last visit: 5/23/2022 Posts: 8 Rating:
|
Yes I have checked the mechanical assembly. Brake release is ok. Reference cam & limit switch operation & repeatability is also perfect. Ball screw and ball nut are also checked. Both are securely attached. And also there is no back lash or axial play/looseness. Actually problem is y axis repeatability is OK untill it is referenced. Once the y axis is referenced level of gantry axis changes. |
Follow us on