1/12/2022 2:55 PM | |
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35924 Rating:
|
I need the article numbers. They begin with 6ED1052 ... |
1/12/2022 2:57 PM | |
Joined: 1/9/2020 Last visit: 7/23/2023 Posts: 21 Rating:
|
and |
1/12/2022 2:59 PM | |
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35924 Rating:
|
You have to LOGO!s with this article number. If yes, I made you a example. |
1/12/2022 3:02 PM | |
Joined: 1/9/2020 Last visit: 7/23/2023 Posts: 21 Rating:
|
Yes, two of those, then three DM16 of the other number |
1/12/2022 3:37 PM | |
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35924 Rating:
|
Here's a simple example.
AttachmentExample two LOGO!s to one web server.zip (497 Downloads) |
2/1/2022 3:29 PM | |
Joined: 1/9/2020 Last visit: 7/23/2023 Posts: 21 Rating:
|
Have it up and running now, cant seem to get the network output from client logo to slave logo to work. Have the logos in master and slave mode. In simulation the network output works from LWE, but the signal wont go to the slave logo. Same subnet. Attatching my project Attachment2 logos Verkstan.zip (286 Downloads) |
2/1/2022 3:45 PM | |
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35924 Rating:
|
You must allow the S7 access in both LOGO!s. File > Properties > Offline settings > General |
2/2/2022 8:27 AM | |
Joined: 1/9/2020 Last visit: 7/23/2023 Posts: 21 Rating:
|
Still no luck, all the flags in simulation works from LWE, but the Q1 on second logo still not active. Then the inputs I1 and I4 are momentary break, works fine in regular simulation, but when I do the online test and activate from LWE the inputs are not red(active) how come? Attachment2 logos Verkstan V2.zip (316 Downloads) |
2/2/2022 9:54 AM | |
Joined: 1/9/2020 Last visit: 7/23/2023 Posts: 21 Rating:
|
Here is the LWE project. Attachment2logos verkstan.zip (302 Downloads) |
2/2/2022 10:41 AM | |
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35924 Rating:
|
Because I have only one LOGO! 8.3, I must change the slave LOGO! to a LOGO! 8.2. Then I chnaged the IP addresses and so on to my addresses. After all this done, I upload the LWE project and the LOGO! programs. And It works. See attached video. AttachmentTest LWE.zip (287 Downloads) |
2/2/2022 3:22 PM | |
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35924 Rating:
|
You have to transfer the variable from LOGO! 1 to LOGO! 2. |
2/2/2022 3:32 PM | |
Joined: 1/9/2020 Last visit: 7/23/2023 Posts: 21 Rating:
|
Hm, how do I do that in example? |
2/2/2022 3:46 PM | |
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35924 Rating:
|
See attachment ...
AttachmentTest.zip (291 Downloads) |
Follow us on