9/6/2022 6:15 AM | |
Joined: 6/23/2022 Last visit: 3/2/2023 Posts: 12 Rating:
|
Hello, I have a project that when opened on my Simatic Manager (Step7 V5.6+SP2+HF9), it does not show the CPU or the program blocks. I can open the Hardware config, but then an error pop up [No changes can be made in this station.] and when I click ok, the CPU from the hardware config disappear. I have installed Drive ES lately, could it be a conflict? I have other projects opening without problem btw. Strange thing is on the Step7(Same version but without drive ES) of my coworkers it opens without a problem. Thanks, J.Noguchi AttachmentNew Document.pdf (1081 Downloads) |
_ |
|
9/6/2022 6:56 AM | |
Joined: 7/2/2015 Last visit: 8/25/2025 Posts: 96 Rating:
|
Hello J.Noguchi, First of all is it an original project or is it a backup from the PLC? And also You can try to do a new project and look if the programm shows you the same issue. If it is, it would be a licence problem or a bad installation
|
If this Information really helps, you could use the Rate function |
|
9/6/2022 7:16 AM | |
Joined: 6/23/2022 Last visit: 3/2/2023 Posts: 12 Rating:
|
|
Last edited by: J.Noguchi at: 09/06/2022 07:28:34_ |
|
9/6/2022 8:47 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, Yes, that is possible Best regards, Wizard |
9/6/2022 12:54 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hi, Here a link for HSP's: Else you should try: STEP 7 V5.6 SP2 / S7-GRAPH V5.6 SP2 / STEP 7 Professional 2017 SR2 Trial Download Best regards, Wizard |
9/9/2022 1:28 AM | |
Joined: 6/23/2022 Last visit: 3/2/2023 Posts: 12 Rating:
|
Hello Wizard, I have updated the HSP without luck. I also did some reasearch on its contents and the CPU I need has a question mark (?) in the article number. I dont know what that means but other items that has a question mark, does not load into the catalog. About the Step7 trial, is there any chance I could endup erasing the license I have when intalling it? Best regards, J.Noguchi |
_ |
|
9/10/2022 7:16 AM | |
Joined: 7/5/2013 Last visit: 9/3/2025 Posts: 3238 Rating:
|
Hello J.Noguchi, the "?" is just a place holder. According New Firmware Version V2.8 for S7-300 CPU 319(F)-3 PN/DP you need HSP 186 (not 200). Regards, Frink |
Last edited by: Prof. Frink at: 09/10/2022 07:19:01Last edited by: Prof. Frink at: 09/10/2022 07:24:32Pi is exactly three! |
|
9/12/2022 4:34 AM | |
Joined: 6/23/2022 Last visit: 3/2/2023 Posts: 12 Rating:
|
Hello Prof. Frink Thanks for pointing it out. In the Configuration with the new firmware: of the link you provided, I followed the link of ID>17581199 on how to download and install the HSP, and did as the guide said, but I ended up back to the HSP download page Wizard had shared already. It seems that the link Wizard shared, should have and is supposed to fix the problem, but it does not... I also tried seaching the HSP 186, but nothing usefull comes up on the browser... Regards, J.Noguchi |
Last edited by: Jen_Moderator at: 09/12/2022 05:55:19Link optimized. _ |
|
9/22/2022 2:39 PM | |
Joined: 6/23/2022 Last visit: 3/2/2023 Posts: 12 Rating:
|
Hi Wizard, Thanks for still making yourself available for this topic. Even after using the HSPS package and updating the HW catalog by selecting all and install all button, CPU still not available, same behaviour as before, I open the project and cannot see program blocks etc. The hardware catalog still the same, there is the folder for the CPU of the project I am trying to open, but it is empty. The question mark I saw is in the HSPS package I downloaded, when manually searching through the files I cold see the CPU I need, but as Prof. Frink mentioned, it is probably just a place holder for other CPUs that use the same firmware. The Drive ES I installed is v5.6 + SP1. Btw when trying to update only the CPU I need, I found out that the HW catalog updater ignores all HSP that has already been supplied within the STEP7, which means I have the file to solve the problem but HW catalog updater wont let me install it as you can see in the attachment. I am guessing the easiest way to solve this is reinstalling STEP7, but I am still looking for a safe way to do that without losing the license key, to be fair I dont even know if this is a valid concern... Best regards, J.Noguchi AttachmentSTEP7 HW catalog update problem.zip (934 Downloads) |
_ |
|
Follow us on