11/8/2006 8:41 PM | |
Posts: 15 Rating:
|
I did not get any answer! NO SUPPORT from siemens in their FORUM! please help me! |
11/13/2006 12:48 PM | |
Joined: 9/29/2005 Last visit: 7/16/2025 Posts: 313 Rating:
|
Hi again, 1. you are right. With Siwatool in demo mode you can only read from your Siwarex modules. 2. Can you ensure that your siwarex lib for the first siwarex ms module is passed through properly by your user program? Because the flashing of the Run-LED can only be envoked when the subroutine SBR_microscale is not called in every cycle. (or the s7-200 is in stop) look also: link (page 7-42) 3. theres no demo version for the microscale libary 4. what happend to your user program when the Run-LED is flashing? Is the weight transfered to the cpu anyhow? do you get any errors via the errorword from the lib? Do you get some errors in step 7-micro/win regarding your s7-200 and modules (/PLC/informaton)... Sorry for that, that i cant give you a final answer, but i am not familiar with your case... |
11/22/2006 6:20 PM | |
Posts: 15 Rating:
|
please send your email to send the file for you for check. Thank you |
11/26/2006 7:01 PM | |
Posts: 15 Rating:
|
this is the project file,check it for siwarex bug. The Bug exist. CPU does not refresh siwarex ms!(RUN lED flashes) Please check the source. AttachmentTR.zip (373 Downloads) |
12/8/2006 10:23 AM | |
Joined: 9/28/2005 Last visit: 10/24/2024 Posts: 414 Rating:
|
[quote user="zani2"]hello Hi, have you read the post 'Can I configure SIWAREX MS without SIWATOOL MS?' |
Smurf |
|