(0)| 3/28/2021 1:40 AM | |
|
Joined: 6/4/2008 Last visit: 11/25/2025 Posts: 1521 Rating:
|
Hi, assuming You have a card reader, plugging it into a windows environment should yield a folder structure as per the attached. If Yes, then it's still possible that it's been corrupted. If not, then You need to ascertain how Your colleague has formatted the card, as it is possible to damage Siemens cards by formatting. Clearly, it's worth attempting regardless unless You have a new card See the link below, unfortunately, V4.6 is no longer downloadable, however, V4.7 is. This does however, mean that if used, a PLC may not be able to communicate any longer until the new version is loaded into the hardware configuration for example. You can download the V4.7 HF35 FIRMWARE here, and simply copy it onto the card. You will then need to load the user data (as per my previous post) on top of the firmware. Regards, Graeme |
Last edited by: Jen_Moderator at: 03/29/2021 11:11:53Optimized link. |
|
This contribution was helpful to
|
|
Follow us on