(0)| 3/19/2021 12:06 PM | |
|
Posts: 22 Rating:
|
Hello there, I have sinumerik CNC With 802D SL. Many times during machine runs one common error we are facing which is 207841 ' AXIS X1 Drive 1 drive: Infeed operation withdrawn' and emergency stop. At the same time in SLM Module Ready Signal becomes Red from green where as all other including of double motor module remains ok and with green Ready LED. As a primary correction we have replaced its SLM Module with same capacity and same parameter. But still we are facing this issue. Because after replacement of SLM Module 1 time this error observed and after reset of error machine run ok from more than 2 hours. The time gap between two alarm is not fixed. Some times comes frequently also. FYI Please, i have attached images of error display. Details of SLM Module : 1) Input 3AC 380-480V 50/60 Hz. 2) Output : DC 600V 17A 10KW. 1P 6SL3130-6AE21-0AB0. Vesion B. Awaiting for your reply how to resolve this issue. Regards, Pranjal Gajjar ------------------------------------------------------------------------------------------ |
Last edited by: Pranjal@9 at: 03/19/2021 12:56:20Last edited by: Jen_Moderator at: 03/19/2021 13:16:58New subject after splitting |
|
| 3/28/2021 7:58 AM | |
|
Posts: 8092 Rating:
|
Hello, I suggest you to caonduct AC in put side power analysis which shall help us to trouble shoot problem. |
Follow us on